Hello:
A designer at a TI focus account we call on sent this message: "We’re using the TLC072. It turns out that with +/-3.15V supplies (the bottom end of our supply voltage tolerance) we actually don’t quite get 5Vpp input and output, which is our design goal. We get closer to 4.5Vpp max output without clipping (into ~12kOhm load). For the design I’ve already completed, we’re just accepting this, but we’d like to improve it in designs that I’m starting right now. "
Hope you all in the business unit can help find a device with better input and output range (it sounds like the output is most important) -- these kinds of searches are very difficult to do without wading thru datasheets. EAU is 100k.
thanks and regards,
George Biner, Arrow LA FAE (TI)