Other Parts Discussed in Thread: TPSI3050-Q1, OPA2991, LM2904B-Q1, OPA310, OPA991, TPSI3050, CSD19534Q5A, CSD19538Q2
Hello,
I am developing an analog voltage measurement 0 .. 10 V that has (besides other) a requirement to have an input impedance between 850kOhms and 900kOhms (for Voltagerange 0V-10V).
This is in powered and upowered state!
For the powered state, OPA2991-Q1 suits very good (low input leakage currents).
The Input divider looks as follows. The factor should be near 1, to introduce the least error caused by the resistances (0,1% already selected)
But in unpowered state the internal protection diode to the positive supply rail (which hat GND-Potential in that case) will conduct and "shorten" R2 and R3.
I already tried to "open" up the connection to the OPA with a FET (driven by a TPSI3050-Q1). This helps, but there the FET drain source leakage current produces the same problem also via the internal protection diode.
My Question:
- Is there a OPA available, with an "absolute" input voltage capability?
Up to 10V would be sufficient. Performance should be similar to OPA2991 (Bipolar supply, low input leakage,...) - If there is no such OPA; is there a FET, with very low drain source leakage current (<10nA)
Thank you
Sebastian