This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC3330: amc3330_sbaa553

Part Number: AMC3330


hi,

in sbaa553 277V is rms voltage and must be divided by 0.7 for peak voltage

therefore peak voltage will be 277/0.7 = 395 Vpeak

and then VLL is about 1.7 * 395  = 671 volt

are i'm true?

best regard

  • Hello,

    The paper describes these parameters. The line-to-line voltage between the two 277V sources is 480V and is reduced to 1V through the split-tap configuration. The equation to get the line voltage is:

    Best regards,
    Eva