Dear TI Teams,
One of our new project need to use a 65W adapter (20V/3.25A). We to detect the signal of the adapter, when the adapter is detected to be inserted, EC will enable INA300 to achieve real-time monitoring of the pressure difference at both ends of PR85 (33mohm).
When the current flowing through both ends of the resistor reaches 3.25A, INA300 pulls down alert #, turns off PQ4945, and thus turns off PQ3. Does this solution feasible? If not, do you have anly better suggestion for this application?
The schematic is show as below, can you help to check it?
Thanks,
Kind Regards