This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2836: 0V voltage output problem

Part Number: OPA2836
Other Parts Discussed in Thread: LM7705

Dear TI Engineer:
I am using the OPA2836 to amplify a signal (0V~0.04V) 77 times(7*11). To get an accurate 0V voltage, whether I had to offset the amplifier's supply voltage by several hundred mV? If so, what is the minimum negative bias voltage? Is it 200mV as stated in the data sheet?
Can I use a Low-Noise Negative Bias Generator like LM7705(output -230mV) as the input of Vs-, and then use a +4.7V power supply as the Vs+ input?