Other Parts Discussed in Thread: AMC3330
Hi, TI teams!
I use three AMC3330-Q1 chips to sense three-phase output voltage of a LC-filter-based converter. However, the high voltage divider circuit does not work properly when dealing with high-frequency components. Do you know the reason? And how can i make the divider circuit work properly?
Here are some informations.
1. The green waveform shows the A-phase output voltage of a LC-filter-based converter (f1 = 50Hz, Amplitude = 50V). The green waveform also contains a 160kHz switching ripple, Vpp=2V, as shown in the zoomed view on the right. The blue waveform shows the voltage of INP - INN. The blue waveform contains a 50Hz 250mV component, which is reasaonable because the ratio of voltage divider is 200:1. However, the blue waveforms also contains a 160kHz component, Vpp = 1.5V. It seems that the switching ripple is not scaled by divider. Why?

2. The schematic diagram and PCB Layout are shown below, which is basically the same as the recommended circuit / PCB layout given in datasheet. The divider network is UP →100KΩ → 0Ω → 1KΩ//1nF → 0Ω → 100KΩ → UN. And the ends of 1KΩ//1nF are connected to INP and INN of AMC3330.

Looking forward to your reply. This problem has been bothering me for several days.