This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9352: Input signal voltage, absolute max

Genius 17645 points
Part Number: TLV9352
Other Parts Discussed in Thread: LM358B, , TLV9102, TLV9152

Hello,

LM358B accepts the input signal voltage exceeding V+ up to 40V.
My customer is looking for a 2ch opamp like it  with lower offset voltage drift and lower offset current drift.

Then I found the below description in TLV9352. 
Does it mean it can allow the input voltage exceeding "(V+) + 0.5V" if the current is limited less than 10mA?

Do we have any other good part numbers?

Regards,
Satoshi Obata