Hi Team,
In my customer's case, OPA192 is configured as high side current sensing circuit, and the Vs+ is coming from the upstream Flyback converter aux winding. The aux winding is unregulated, so Vs+ will shift between 18V and 21V based on the different loading on aux winding, and my customer observed that OPA192's output voltage will also shift when Vs+ is shifting.
Is this behavior related to P/N transition region? Or it it more related to PSRR?
According to OPA192 datasheet, P/N transition happens betwwen (V+) – 3 V and (V+) – 1.5 V, will this rule apply to all supply voltage range?
Regards,
Charles