Part Number: OPA170
Other Parts Discussed in Thread: OPA310
Hi Team,
Siemens is looking for an alternative for OPA170 without ESD protection diodes. Do we have such a device available?
Thanks, Stefan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Stefan,
What is the supply voltage?
The OPA310 has fail-safe ESD protection that allows the input pins to pin larger than V+ without damaging the device. The OPA310 is a low voltage device (5.5) and the OPA170 is a high voltage device (36V). Fast Enable Amplifier With Fail-Safe Input ESD
All the best,
Carolina
Hi Caro,
Thanks for your support. Since the supply voltage is 3.3V, the OPA310 sounds for an good option here.
Best, Stefan