hi,
The schematic diagram is shown in the following figure. The maximum input voltage of the pin is 14.7V. If the VCC3 voltage is too high, will the operational amplifier burn out? For the same output current, reducing the input voltage requires increasing the R10 resistance value. The R10 resistance value should not be too large, which will increase power consumption and may also cause the resistance to burn out. Is there a good solution? Is there a good improvement plan for the circuit diagram?

Thanks!