This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC272: Voltage abnormal

Part Number: TLC272
Other Parts Discussed in Thread: OPA2374

Hi team,

My customer use TLC272 for voltage follower in the follow SCH, they found the output voltage waveform is very different from V+ input waveform.

And when Vin=5V, the P-P value of waveform is about 4.2V.(blue: pin5 voltage; purple:pin7 voltage; green: pin7 voltage after filter )

when Vin =8V, the P-P value  of waveform is about 2.5V. 

when Vin =0, the P-P value  of waveform is about 0. seems normal.

So could you help to analysis the possible reason for this phenomenon? and is it normal phenomenon? because it doesn't leads to clear issue. But the waveform is abnormal.