This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: The problem of significant gain drop with increasing frequency in the use scenario of large feedback and input resistors

Part Number: LMH5401

Tool/software:

The circuit when we use LMH5401 are as follow picture

We built a model in ADS for simulation of this usage. The model of LMH5401 is achieved from the official website. The models of PCB wiring and coaxial lines are achieved from simulation extraction and vector network analyzer measurement, respectively. The relationship between the simulated gain and frequency is shown below

However, when testing on actual PCB, we found that the gain of this network would sharply decay with increasing frequency, as shown in the following figure

The difference between the maximum and minimum gain within 300MHz is about 6dB, which cannot be accepted. What is the reason for this problem? Also, is there any way to optimize it?

Thanks