Part Number: INA214
Tool/software:
Hi Team
Customer is using INA214 as output current sense in a industry power supply project at low side. they found there is one pcs of total 3pcs which output will be 2V which will trigger OCP to cause the power start-up failure at -25 ℃ ambient temperature. but there is no current on load.
and the output will be zero when increase the ambient temperature to 25℃ and everything works normal. It is tricky for customer.
Can you show your insight what is the possible root-cause of this issue or what we should do next step yo identify the root-cause