This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA331: INA331

Part Number: INA331
Other Parts Discussed in Thread: OPA336, INA351, LM7705, OPA333

Tool/software:

For instrumentation amplifier, INA331, this is being used as differential amplifier with R1 = 100K digipot and R2 = 100K. From DS, this indicates that VREF requires to be driven with low impedance input. To acheive low impedance for VREF, this has been implemented as follows:

Digipot, L connected to 0V.

Digipot, W connected to input of buffer, OPA336, with output connected to VREF

Digipot, W connected to RG input on INA331 along with one side of R2, 100K. Other side of R2 connected to Vout.

Please advise if above configuration outlined allows:

Varition of Gain as digipot is used as variable resistor in expression, G = 5 + (5R2/R1)

VREF is driven from low impedance, OPA336

If you are able to provide an update ASAP please ?

Thanks