OPA2994: The best op-amp option to drive capacity load

Part Number: OPA2994
Other Parts Discussed in Thread: OPA994

Tool/software:

Hi team,

Just want to make sure, if the customer want to need op-amp to drive capacity load, is OPA2994 the best option? Their requirement is as below:

supply voltage: +/-4.5V

Input range: +/- 2.5V

Gain: +/- 1

Load Capacitor: 0-5uF

Drive Current: 0.1mA-5mA