Part Number: LM358B
Other Parts Discussed in Thread: LM2904B, LM358
Tool/software:
About the LM358 Spice Model (LMx58B_LM2904B)
Set the V+ power supply to +5V.
When the V-power supply is set to 0 V to -1 V, the OPAMP output is stuck close to the V+ power supply voltage.
V- Normal operation when power is -2 V or less.
Can the actual product operate with a single power supply structure with a V-power supply connected to GND? Also, is it possible to do a simulation when the actual product is operational?
(V-) -1.5V OK : 0V(GND) NG