Other Parts Discussed in Thread: OPA2180
Tool/software:
Hi eyeryone, I am designing a howland currents source which suppose to output -4mA to 4mA constant current through R9 while the Vin is 0v to 5.2v. On LTspice simulation it works fine, but in reality it doesn't produce enough current through R9 and the current isn't symmety as well (2.7mA to -4.7mA) ... I tried to change the resistance of R10 but did not work well, should I use another op-amp or is there something went wrong in the circuit?
Thank you very much in advance and best regards.