Part Number: INA129
Tool/software:
Hi TIer
Could you help to check INA129 simulation models can be imported properly into TINA?
Customer get the failure. Thank you very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA129
Tool/software:
Hi TIer
Could you help to check INA129 simulation models can be imported properly into TINA?
Customer get the failure. Thank you very much.
Customer testbech is :
The customer said that his simulation has no output, but it is OK to use the TINA simulation file TI provided. May this problem occur when importing lib?
The customer wants to amplify the AC signal, please help to see what the difference is.
Thank you very much.
Hi Yuxi,
There are two options. One is to double click on the output measurement probe VF1 in the schematic and set the IO state to be output (see image below). Or download the reference design from the link below and copy the model and paste it into their simulation and replace the one that is currently in there.

Best Regards,
Chris Featherstone