Tool/software:
Sir,
1) Is there any Power Amplifier Module with TI as Evaluation kit whose O/P is 43 dBm/20W for I/P of -15 to -10 dBm (Frequency Range: 2.4 to 2.8 GHz)
2) If the above PA is not available as single module(Evaluation Kit), Pls. suggest us the combination of Power amplifier ICs which are to be used to get 20W O/P power for I/P of -15 to -10 dBm
Pls. don't consider the above given part no. which was mention as mandatory field.
Regards
Durga Prasad,
DRDO