Other Parts Discussed in Thread: PGA849, PGA281, PGA280
Tool/software:
The input signals can vary from ±10V, ±5V, ±1V, and ±500mV, with a frequency range of 0-30kHz.
The given ADC's reference voltage (VREF) is 4.096V and its requirement for differential inputs(inputs range is
-4.096~+4.096), Is the PGA855 an appropriate choice? or it has a better choice.