Other Parts Discussed in Thread: LMV321
Tool/software:
We have a specific case that we need some clarification.Normally, our circuit is functioning with 3.3V on Inputs and 3.3V on Outputs, but we have some units where the component have 3.3V on Inputs and 2.8V on Outputs
We did a Swap ABA in under to review if the failure is following the component or the unit and the component still failing in a Know Good Unit, so we need to understand why the component is not functioning as expected? The pin 3 of the component is it used to feedback function? Which voltage will i need to see reflected on Outputs?