Other Parts Discussed in Thread: LMP8601
Tool/software:
We are using LMP8601QMAX device.
It has been working fine during the validation testing for the past few weeks.
During the validation, suddenly the LMP8601 output goes to 0V then we analyzed and found that supply voltage itself goes to 0V after power up.
So during debugging we found that the impedance across the +5V supply and GND is reduced to 1.5 Ohm. After lifting the Pin 6 (i.e., Vs pin of LMP8601QMAX) the impedance increased to normal range (as like previous working condition i.e., 4.5K ohm) and also 5V is properly generated by the power regulator.
Still this 1.5Ohm resistance is observed between Pin 6 (Vs) from the pad and GND after lifting the pin .
So, kindly let me know the possible conditions which could cause the short between Vs and GND pin within the device.
Regards,
Devendhiran K