This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO224: Isolation design

Part Number: ISO224

Tool/software:

For our  new  project, we need the electronics that comes into contact with the patient being treated to be isolated from other components of the medical device. The isolation voltage should be 5KV or higher. The signals to be isolated are:

  1. Digital control signals, +3.3V, with frequency lower than 5 KHz.
  2. Output voltage +/- 4V max, frequency lower than100 Hz

Can you recommend a component to implement point 1?

Can point 2 be implemented by the ISO224? Do we need to  provide positive and negative power supplies on both the isolated and the non isolated sections of the ISO224?

Thank you 

Martin Grinfeld