Part Number: OPA187
Other Parts Discussed in Thread: OPA205
Tool/software:
My application uses the OPA187 with (V-) = 0V, (V+) = 12V. It is configured as a non-inverting amplifier. I would like to know if an output voltage of 0.5V at 5mA load current is within the linear output swing range of the device?
The TI precision labs video on op-amp output swing (https://www.ti.com/content/dam/videos/external-videos/en-us/1/3816841626001/6279999026001.mp4/subassets/opamps-input-output-limitations-output-swing-presentation-quiz.pdf) suggests that conditions for the open-loop voltage range specification can be used to determine the linear output swing range. The open-loop voltage gain is specified from (V-)+0.3 to (V+)-0.3. However, this for a 10kOhm load, which is a far lighter load than my application.
![]()
Figure 10 in the datasheet show the output voltage swing at 5mA output current. But based on the response to Danilo's question, this for a much lower supply voltage (Vs = +/-2.75V) than my application. Is there a similar plot of output voltage swing vs output current for the OPA187 in high-voltage operation?