Other Parts Discussed in Thread: AMC1351, AMC3330
Tool/software:
Hi All,
I am considering using AMC1350 (datasheet) for the three-phase AC line-to-line measurements. It has ±5V input, ideal for AC signals,
According to the recommended schematics from the datasheet, the GND is connected to the low side of the last resistor in the voltage divider, and the high-side VDD1 to GND1 should be max. 6.5V. The example in the datasheet is for measuring line-to-neutral (i.e., earthed), Figure 8-1.
But in my case (when connecting line-to-line voltage to measure motor output 400-690Vac), I have both lines at Vll/√(2) to ground, so in that way, my high-side VDD1 to GND1 will be more than 6.5V.
Is it possible to measure line-to-line voltage using AMC1350, and what would the connection circuit look like?
One more question: the figure below shows the input and output voltage range, where input is +/-5 V and output is +/-2 V. Is there any scaling in the block?
Kind regards, MB