This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-3PHGANINV: [3PHGANINV+TMS320F28379D] Please help me!! check the inverter output waveform.

Part Number: BOOSTXL-3PHGANINV

Tool/software:

I connected F28379D and 3PHGANINV.

F28379D  to  3PHGANINV

J5       ----        J1       

J7       ----        J3

J6       ----        J2

J8       ----        J4

The signal output of EPWM 1a to EPWM 3b of F28379D is designated as numbers 80 to 75 of F28379D.
The output waveform has been confirmed.

Numbers 80 to 75 of F28379D are connected to numbers 40 to 35 of 3PHGANINV.

I created a PWM signal using the DEADBAND example on F28379D. Then, I checked the output waveforms at Va, Vb, and Vc of 3PHGANINV on an oscilloscope.
There was no waveform on the oscilloscope.

Do I need to write a separate code to check the output waveforms in Va, Vb, and Vc of 3PHGANINV?
(A power supply was used as an external power source.)
I am studying the servo-Axial-drive example. Do I have to modify this example to see the output waveforms in Va, Vb, and Vc?