Part Number: TLV3701-Q1
Other Parts Discussed in Thread: TLV1851-Q1
Tool/software:
The datasheet states (clearly) that the device's input common mode range extends up to Vcc + 5V. But not a single performance graph or specification mentions operation with a common mode above Vcc.
Moreover, on page 2, the datasheet states:
"For harsh environments, the inputs can be taken 5 V above the positive supply rail without damage to the device."
To, this sounds like a guarantee of survival, not of correct operation.
I have the impression that the author of the datasheet has confused input voltage range and common mode range.
Can you please clarify?
More precisely, I wonder if the circuit below will always generate a high output if the node at P517 goes above +5V (while staying within the Vcc+5V range).
Best regards,
Eric