Other Parts Discussed in Thread: TLV9002, LM2904BA
Tool/software:
Dear Team,
We are using above mentioned OP-Amp (LM2904BAQPWR1) in our proto circuit.
The supply voltage for the IC is 3.3V.
When we are testing the Op-amp, It is observed that output not crossing 2V once input crosses certain range.
1. Is it possible to get output more than 2.5V for this device using 3.3V supply? If Yes, How we can achieve it?
2. If its not possible to get the output more than 2.5V , could you please suggest the alternate IC with exact same footprint ?
Kindly support us with this query , as we are in final stage of development.
Thanks & Regards.