Part Number: AMC3311-Q1
Other Parts Discussed in Thread: AMC23C11, AMC3311
Tool/software:
I am doing simulations for AMC3311 and AMC23c11 for my voltage sensing application on TINA TI. When I connect the recomenned decoupler capacitors, VDD is 5V LDOout is 2.9V so DCDCout is 2.75V and HLDOout is 2.67V. This has to be okay for the device but it operates as fail-safe mode. Its not under the undervoltage limits. When I bypass the LDOout and give DCDCin 3.3V directly the system oparates normally. Could it be an error on simulation or is it normal?