Part Number: PGA308
Other Parts Discussed in Thread: INA333, PGA309
Tool/software:
Hello TI Support Team,
We are currently experimenting with the PGA308 as a replacement for an INA333. The goal is to change things like offset and gain without additional soldering.
If I understand correctly, each PGA308 has individual inaccuracies. Therefore, each PGA must be calibrated with the system?
All the calibration procedures I have found so far (PGA309 / PGA308) use the actual stimuli of the sensors. Here, the minimum and maximum values of the sensor must be applied to the component in real life. This is not possible in our application (strain gauges).
It becomes even more problematic when our system is used by customers. Here, only the range in which the measuring bridge is detuned is given.
Therefore, I experimented with the formulas from the application note. However, when I load the calculated register values into the PGA, the output is always a few mV off. I think this is due to the manufacturing tolerances of the ICs mentioned above.
Is there a way to measure the PGA in advance with a bridge simulator (0.25 mV/V, 0.5mV/V, 1mV/V, 2mV/V, 4mV/V, 5mV/V, 8mV/V, 10mV/V, 25mV/V, 50mV/V) and determine an individual error from it?
This error could then be included in the calculation to obtain a more accurate output value for real settings, e.g., 2.38mV/V. Is there perhaps already a corresponding set of formulas including such a correction value?
Best regards,
Sven