Other Parts Discussed in Thread: TLV3201-Q1, TLV3201, LMV762,
Tool/software:
I want to replace the LMV762QMMX/NOPB with the TLV3201-Q1.
Can you tell me if the Alternative TLV3201-Q1 needs more or less supply current in the same application?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I want to replace the LMV762QMMX/NOPB with the TLV3201-Q1.
Can you tell me if the Alternative TLV3201-Q1 needs more or less supply current in the same application?

Hello Patrick,
The TLV3201 is less current at higher speed.
The TLV3201 is 50uA max, and the LMV762 is 700uA max - almost 10x more.
| ► Part Number | LMV762QMM/NOPB | TLV3201AIDCKR |
| Manufacturer | TI | TI |
| Pinout | Dual | Northwest |
| Channel Count | 2 | 1 |
| Package | VSSOP-8 | SOT-SC70-5 |
| Package (TI Equiv) | DGK8 | DCK5 |
| Vs min (V) | 2.7 | 2.7 |
| Vs max (V) | 5 | 5.5 |
| Response Time, typ (µs) | 0.12 | 0.045 |
| Vos max 25°C (mV) | 1 | 5 |
| Input Range | To V- | R-R |
| Output Type | PP | PP |
| IQ (max) (mA) | 0.7 | 0.05 |
| IBias (typ) (nA) | 0.0002 | 0.001 |
| Temperature Min | -40 | -40 |
| Temperature Max | 125 | 125 |
| Additional Features | Int 1.2mV hyst | |
| Auto Qual | Q1 | |
| GPN | LMV762Q-Q1 | TLV3201 |
| Datasheet | LMV762Q-Q1 | TLV3201 |
| TI Web Page | LMV762Q-Q1 | TLV3201 |