Tool/software:
Kindly share the Maximum reflow for both components
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Jeya,
The OPA328DBVR MSL rating / peak reflow is Level-1-260C-UNLIM.Please see attached the OPA328DBVR Quality, reliability & packaging data on the attached PDF file.
The INA310A3IDGKR MSL rating / peak reflow is Level-2-260C-1 YEAR. Please see attached the INA310A3IDGKR Quality, reliability & packaging data on the attached PDF file.
Thank you and Best Regards,
Luis
Hi,
Thanks for the response
Could you share the maximum Reflow cycle of both component
Regards
Jeya Dharani
Hi Jeya,
The MSL peak reflow temperature for both OPA328DBVR and INA310A3IDGKR is 260°C. The IC packages are classified according to J-STD-020 and withstand three reflow cycles.
Below is a link to an Application Report explaining the relationship of MSL rating to the customer production floor life and surface mount reflow temperatures for TI semiconductors. Figure 3 on the Application Note illustrates the temperatures and times associated with the different Reflow oven zones.
MSL Ratings and Reflow Profiles

Let me know if this does not answer your question.
Thank you and Best Regards,
Luis