Other Parts Discussed in Thread: TLV1822, TLV1832
Tool/software:
Hello,
I use the TLV1822 in a signal chain for a detection of a 15 V square wave signal up to 25 kHz:


Above approximately 18 kHz the upper channel, that detects the high-threshold, stops switching and remains in high impedant state, while the lower channel, that detects the low-threshold, still woks. Another device in a similar circuit shows the same behaviour.
Here channel4 (green) the input at pin 2 and channel 1 (yellow) the output at pin 1 at working frequency of 12 kHz:

The same measurement at 20 kHz with the output in high-z:
And now instead of the output the second input at pin 3 at channel 1 (yellow), while no switching occurs:

I cannot find any reason in the datasheet, why this shouldn't work.
In a former design I used the LM2903D with exactly the same conditions without any problems.
Do you have an answer?
Best regards,
Christian