This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC3330: AC Frequency Measurement

Part Number: AMC3330

Tool/software:

Hello,

Can AMC3300 measure AC phase voltage  as well as 400hZ frequency?

The output bandwidth of AMC3300 is minimum 300kHz, so can I measure up to this frequency?

  • Hi Ilgin,

    The AMC3300 can measure 400Hz frequency and can measure AC phase voltage. 

    Any frequency after the typ value of 375kHz will lead to more attenuation on the output. As long as the frequency is below the min output bandwidth, the measurements should be okay. 

    Thanks,