Part Number: TLV1814-Q1
Other Parts Discussed in Thread: TLV1814,
Tool/software:
Hello TI forum,
The task at hand is to buffer a Hall effect sensor output signal. The sensor cannot reliably source enough current on its output channel, so a comparator seems like a good solution - it will provide any necessary current sourcing capability, and it should have the added benefit of not nearly as much noise on the output. The Hall sensor output switches digitally between 0V and 5V, and the comparator would be powered off of 5V.
The concern is that, since the Hall effect sensor will be transmitting in a noisy environment with plenty of EMI, the Hall sensor input may swing beyond 5V and below 0V. As an example comparator, the TLV1814-Q1 has a common-mode voltage range of just ±0.2V compared to the supply voltage, which leaves almost no margin for input signal fluctuation in the case of this application.
Are there any ways to mitigate or eliminate the risk of violating the CMVR in a noisy environment for comparators? Or is there a line of similar comparators with more acceptable CMVR tolerance?