Other Parts Discussed in Thread: OPA2374
Tool/software:
Hello,
I am currently working on a project where I am using the TLV9062 operational amplifier in a buffer configuration to read a voltage pulse with an MCU. The input pulse ranges from 0 to 2V, with a duration between 50 µs and 300 µs, at a frequency of 1 Hz.
To allow the MCU enough time to read the output voltage, I have added a 100 nF capacitive load at the output of the op-amp. However, I am experiencing significant voltage spikes at the output, particularly near 0V, while the spikes are less pronounced near 2V.
To improve stability, I added a resistor in the feedback loop, which slightly reduced the spikes, but the results are still not optimal. The spikes are too high near 0V and weaker near 2V.
When testing with the OPA2374, I noticed that the voltage spikes are much less pronounced. However, I understand that Texas Instruments recommends using the TLV9062 for new designs, and I would prefer to use it if possible.
Could you advise on the optimal circuit design to avoid these voltage spikes in my case? Is there a better configuration to stabilize the buffer (e.g., resistor values or additional components)? Alternatively, I am open to suggestions for other op-amp references that may be suitable for my application.
Thank you for your help!