This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA296A-Q1: Maximum current is 100A for 10 seconds

Part Number: INA296A-Q1
Other Parts Discussed in Thread: INA229

Tool/software:

I would like to request a circuit design review.

After reading the current value through INA296A2QDDFRQ1 and comparing it through TLV9024QDYYRQ1.

The output value is controlled through SN74AHC1G08QDBVRQ1.

Discharge up to 100A for 10 seconds

Therefore, in this case, the output value of TLV9024QDYYRQ1 is 4.5V.

In this case, you need to compare the voltage with PIN 11 of TLV9024QDYYRQ1.

Maintain 100A for 10 seconds and at 10 seconds, 13PIN of TLV9024QDYYRQ1 should output 0V.

Therefore, the 10PIN of TLV9024QDYYRQ1 must be maintained for 10 seconds. Please provide guidance on this part.


In addition to the information mentioned above, please review the remaining circuit diagram.

(VCC: 5V / VCC load up to 400mA)
The shunt resistance value is 1m ohm. / 

Voltage is up to 56Vti_FINAL.pdf