This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO224: the input voltage range and power supply voltage range

Part Number: ISO224

Tool/software:

Hi Team,

Usually, the amplifier input voltage range is limited by power supply voltage range. But the ISO224 datasheet describes when the VDD1 is 5V, the input voltage range can be up to ±12V. Why? Is there any special design in the chip? 

If the input voltage range is ±12V, can I only apply 5V in the VDD1. Many thanks.