This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240-Q1: Output short fails to ground

Part Number: INA240-Q1


Tool/software:

Hello,

I'm currently using INA240-Q1 to retreive the current value from a 500 uOhm shunt resistance. Voltage drop across the shunt resistor is up to 24 V, with peaks of 70 A current. However, besides being in the common mode ranges for the input pins and being the INA240-Q1 powered with a 5 V supply, the device fails and the output shorts to ground.

Any clue on what might be the cause?

Thank you in advance,

Luca