This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA225: Equalent IC for INA225AQDGKRQ1 with high voltage input(48V application)

Part Number: INA225


Tool/software:

Hi,

I am using the INA225AQDGKRQ1 IC in one of my circuit for the Current measurement, the circuit input voltage is 24V

Now i have requirement for the higher input voltage as 48V, this Part No.INA225AQDGKRQ1 will not support for the 48V I/P Application. I am in a position that i can't change my PCB Layout. Can you suggest me a Equalent part no(Pin to Pin replacement) to support the current sending for 48VDC input: