Tool/software:
Hi, what is the behavior with the input pin when the Vcm goes above 2V?
It will clamp the voltage of the input will be still high impedance?
LMV393MM-NOPB

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, what is the behavior with the input pin when the Vcm goes above 2V?
It will clamp the voltage of the input will be still high impedance?
LMV393MM-NOPB

Hi Fabio,
Since the Abs Max states an absolute 5.5V, there is not a upper ESD clamp.
So it should remain high impedance up until 5.5V, then you get into the range where there could be a breakdown at a higher voltage (No, we do not comment on that breakdown voltage as it is way out of DS specs).
At about 800mV below V+, the bias current will start to drop into the pA's as the input stage gets cut off.