This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3605: Input differential mode resistance range

Part Number: TLV3605

Tool/software:

Dear E2E,

I am using this comparator in an application where a signal is fed to the positive comparator input and a reference signal is fed to the negative comparator input. The reference signal is generated by a voltage-output DAC. To minimise the cost of the DAC, I'm using a 8-bit DAC, with a voltage divider scaling-down the DAC output voltage into a range of about 0V to 0.1V. This voltage divider effectively increases the system's reference voltage resolution to that of a 12-bit DAC without voltage divider. 

I am trying to work out what values to use for the resistors in the voltage divider. In the TLV3605 datasheet, the input-differential-mode resistance Rdm is specified as typically 67k. This resistance will be in parallel with the bottom resistor of the potential divider. But the Rdm spec has no min/max, only typical. 

Please could you advise what are the min/max range of the Rdm?

Many thanks,

Ben