Other Parts Discussed in Thread: PGA849, PGA855
Tool/software:
Hello,
I am seeking guidance regarding the PGA280. Specifically what the input min max voltage range is for the SPI signals. The datasheet is somewhat ambiguous. It states that Signal input terminals, voltage cannot exceed VSN - 0.5 to VSP + 0.5. There is no distinction between the analog input signals or the digital input signals. In my case this would be +/-15.5V, but my DVDD is equal to 3.3V. It is uncommon to see digital signal's spec'd to tolerate voltages much beyond DVDD so this is suspicious. I guess the question is if the absolute max rating listed as "Signal input terminals, voltage" applies to all inputs on the device, and if it does not apply to the SPI signals, what is the absolute rating?

(Page 39 of datasheet)