Tool/software:
Hi,
I'm Using the INA237 for a current monitoring and load switching application, I shared the schematics down below, What I'm trying to do here is to configure the INA237 to work standalone and detect the current limit of let's say 8A on the load and when it reaches to the limit, the alert pin is configured to latch a relay which disonnects the load.
I'm using a host MCU to configure it using I2C and it works for a couple of hours but after that suddenly the alert pin triggers even if the current is not reached the limit.
The first thing I'm wondering to know is if there is an issue with hardware or the way I'm using it.