Other Parts Discussed in Thread: PGA849, PGA280, INA500,
Tool/software:
Hello,
I would like to use the PGA855 with a single supply and a signal of +/- 4V with a common-mode voltage of 2.5V. My question is: does "Input voltage (V_I)" of 7.5 Electrical Characteristics mean the Common-mode input voltage or the voltage of IN+ and IN- individually? Reading "Input voltage", I would assume the latter, but this seems to contradict figures 9-1 to 9-5. Furthermore, the similar-looking PGA849 has "Common-mode input voltage" in the same place in the table.
Is this a good amplifier for this application? I want something simple (I like A0 A1 A2 over SPI), with a single channel, and below unity gain options. I think the PGA855 is intended for slightly higher voltage applications, but it's the closest thing I could find. Any recommendations would be much appreciated.
Thanks,
Marcel