TLV9062: Why in the simulation the input signal can be higher than V+

Part Number: TLV9062
Other Parts Discussed in Thread: TLV9064

Tool/software:

Hi team,

The customer had a request with 0~1.8V input signal and inverting function circuit to output -1.8V voltage. They decided to use +1.8V and -3.3V as power supply. I make a simulation and it works. 

But when I set the positive power as 0, it still works. I don't understand the reason. Could you help explain the reason? 

From the datasheet, the input signal should be lower than (V+)+0.1.So when the V+ is 0, I guess that it shouldn't work. Could you help check the reason?