Other Parts Discussed in Thread: LAUNCHXL-F28379D, BOOSTXL-AFE031
Tool/software:
Hi sir,
i'm trying the integrate the BOOSTXL-AFE031 MODULE along with a LAUNCHXL-F28379D launch pad to a 28v DC line.but it is not working properly.
i followed this thing and made similar setup.
and i'll provide u the output waveforms i'm getting at TB1.
THIS is when not integrated with powerline ( the 28v input is off)
this is when 28v dc line is on.
can u help me in identifying the problem here.
i'm using 28v 1.5A light as a load. along with this i'm using the capacitors and inductors which are mention in
the document .