Tool/software:
I am using the IC with 2.048V reference. While doing over voltage test, there is a sudden rate of change of voltage at the input of IC. While doing so, the output is getting stuck at a particular voltage (let say 3.2V).
1. What is the maximum dv/dt is allowed at the input of INA240-A2?
2. What could be the expected output when the Common mode voltage exceeds 80V?