Tool/software:
Hi,
I wondered if you have a typical (transient) startup time for the AMC3301-Q1 from application of the VDD input (3.3Vdc) to get to a stable output signal from the device?
Also, looking at the data sheet for the AMC3301-Q1, am I correct in thinking that the maximum VDD current draw is 42mA and a typical current draw should be around 28mA on the VDD pin if using a 3.3Vdc supply?
Kind regards
Michael