This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3491: Interference occurs even without input and when there is a 30 MHz signal. It seems to be caused by self-excitation.

Part Number: THS3491


Tool/software:

Circuit diagram:

Output without input signal:

Output with 30MHz burst input signal:

How to resolve this problem?